2018-04-22 5:39 AM
Hi there!
I have a bit of code, which was initialized using CubeMX and now I want to use a mix of HAL and LL (use LL for transmitting, use HAL for everything else).
Currently I have tried to generate CubeMX code and just add manually the stm32f4xx_ll_spi.c/h files, then I include the header where I need. I want to replace this function:
void spi_write(uint8_t data) {
HAL_SPI_Transmit(SPI_PORT,&data,1,HAL_MAX_DELAY);}With this one:
void ST7735_write(uint8_t data) {
LL_SPI_TransmitData8 (&hspi2, data); while (!LL_SPI_IsActiveFlag_TXE(&hspi2)) { ; }}But it does not work. I also get an error regarding hspi2, because it is of type 'SPI_HandleTypeDef' and not 'SPI_TypeDef'. Does anyone have any idea what I am missing? Thank you!
#ll #spi #hal2018-04-22 5:52 AM
I managed to get rid of the error by using (&hspi2)->Instance instead of simple hspi2. But I still cannot transmit data.
I have also tried to leave the LL drivers and work directly on the registers, but it does not work.
(&hspi2)->Instance->DR = data;
while (!((&hspi2)->Instance->SR & ((uint16_t)0x0002))); //Check TXE flag while ((&hspi2)->Instance->SR & ((uint16_t)0x0080)); // Check busy flagWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.