2013-06-23 6:37 PM
Hey,,
I want to implement TCP/IP using no OS on MCBSTM32C (STM32F107VC). The driver ETH_STM32x.c file writen by KEIL uses RTX functions in it's receiving part. <i>Therefore i wrote my own function for receiving a frame, everything else is similar to the driver.</i>But it is not working. After a lot of checking,<b> i realised it gets stuck at a certain point(second if condition of loop). The issue is , the DMA OWN bit in the descriptor is never reset. why is this problem arising. </b>Please Help !!!my receiving function returns the packet length and it writes the data from address:packet .it returns 0 otherwise.<pre> U16 receive_packet( U8 * packet){U32 i,RxLen;U32 *sp;i = RxBufIndex;if (ETH->DMASR &DSR_RS ==0) // check if a packet has been received and buffered{ return 0;}if((Rx_Desc[i].Stat & DMA_RX_OWN) != 0){ return 0;} if( (Rx_Desc[i].Stat & DMA_RX_ES ==0) && ((Rx_Desc[i].Stat & DMA_RX_SEG_MASK) == DMA_RX_SEG_MASK)){ RxLen = ((Rx_Desc[i].Stat >> 16) & 0x3FFF) - 4; sp = (U32 *)(Rx_Desc[i].Addr & ~3); for (RxLen = (RxLen + 3) >> 2; RxLen; RxLen--) { *packet++ = *sp++; }}else{ RxLen=0;}Rx_Desc[i].Stat = DMA_RX_OWN; // Set Own bit of the Rx descriptor Status: gives the buffer back to ETHERNET DMA if (++i == NUM_RX_BUF) i = 0; RxBufIndex = i;if (ETH->DMASR & INT_RBUIE) { ETH->DMASR = INT_RBUIE; // Rx DMA suspended, resume DMA reception. ETH->DMARPDR = 0;}ETH->DMASR = DSR_NIS | DSR_RS ; // Clear the interrupt pending bitsreturn(RxLen);}</pre> #mcbstm32c-stm32f107vc-ethernetWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.