2022-08-26 11:30 AM
in main.c
int connectionClosed = 0;
...
Setup routine of socket
...
while(1){
sin_size = sizeof(struct sockaddr_in);
new_socket = lwip_accept(s_create, (struct sockaddr *)&client_addr, &sin_size);
if (new_socket > 0){
msgSize = sprintf(printMsg, "New client connected from IP: %s, Port: %d\r\n", inet_ntoa(client_addr.sin_addr), ntohs(client_addr.sin_port));
HAL_UART_Transmit(&huart3, (uint8_t*)printMsg, msgSize, 10);
connectionClosed = 0;
while(strncmp(recvBuff,"close", 5)){
if (connectionClosed) {
goto socket_close;
}
memset(recvBuff, 0, sizeof(recvBuff));
retVal = lwip_recv(new_socket, recvBuff, sizeof(recvBuff), MSG_DONTWAIT);
// Process buffer
processMsg(recvBuff);
//Toggle LED every ~second
updateLED();
osDelay(1);
}// End of client connected loop
socket_close:
lwip_close(new_socket);
}
}
in sockets.c
extern connectionClosed;
static void
event_callback(struct netconn *conn, enum netconn_evt evt, u16_t len)
{
int s, check_waiters;
struct lwip_sock *sock;
SYS_ARCH_DECL_PROTECT(lev);
LWIP_UNUSED_ARG(len);
/* Get socket */
if (conn) {
s = conn->socket;
if (s < 0) {
/* Data comes in right away after an accept, even though
* the server task might not have created a new socket yet.
* Just count down (or up) if that's the case and we
* will use the data later. Note that only receive events
* can happen before the new socket is set up. */
SYS_ARCH_PROTECT(lev);
if (conn->socket < 0) {
if (evt == NETCONN_EVT_RCVPLUS) {
/* conn->socket is -1 on initialization
lwip_accept adjusts sock->recvevent if conn->socket < -1 */
conn->socket--;
}
SYS_ARCH_UNPROTECT(lev);
return;
}
s = conn->socket;
SYS_ARCH_UNPROTECT(lev);
}
sock = get_socket(s);
if (!sock) {
return;
}
} else {
return;
}
check_waiters = 1;
SYS_ARCH_PROTECT(lev);
/* Set event as required */
switch (evt) {
case NETCONN_EVT_RCVPLUS:
sock->rcvevent++;
if (sock->rcvevent > 1) {
check_waiters = 0;
}
break;
case NETCONN_EVT_RCVMINUS:
sock->rcvevent--;
check_waiters = 0;
break;
case NETCONN_EVT_SENDPLUS:
if (sock->sendevent) {
check_waiters = 0;
}
sock->sendevent = 1;
break;
case NETCONN_EVT_SENDMINUS:
sock->sendevent = 0;
check_waiters = 0;
break;
case NETCONN_EVT_ERROR:
sock->errevent = 1;
connectionClosed = 1;
break;
default:
LWIP_ASSERT("unknown event", 0);
break;
}
if (sock->select_waiting && check_waiters) {
/* Save which events are active */
int has_recvevent, has_sendevent, has_errevent;
has_recvevent = sock->rcvevent > 0;
has_sendevent = sock->sendevent != 0;
has_errevent = sock->errevent != 0;
SYS_ARCH_UNPROTECT(lev);
/* Check any select calls waiting on this socket */
select_check_waiters(s, has_recvevent, has_sendevent, has_errevent);
} else {
SYS_ARCH_UNPROTECT(lev);
}
done_socket(sock);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.