2016-05-27 2:08 AM
Hi,
Just been testing some software that uses the STM32CubeF4 version of lwIP 1.4.1 stack. With asserts enabled we were very occasionally seeing one triggered in pbuf.c:950. LWIP_ASSERT(''pbuf_free: p->ref > 0'', p->ref > 0); For info this part of code is enclosed in a SYS_ARCH_PROTECT/SYS_ARCH_UNPROTECT block, but as SYS_LIGHTWEIGHT_PROT was 0 it was not protected. Looking into the lwIP docs I see that when using an OS/interrupts you should really define SYS_LIGHTWEIGHT_PROT to 1 so that the relevant block is protected. If I define SYS_LIGHTWEIGHT_PROT to 1 in our code we see no more asserts. A quick grep of ST sample code and I see that SYS_LIGHTWEIGHT_PROT is always 0. Is this really correct ? Did a quick check of an older project that used another vendor Cortex-M3 product and they actually checked that SYS_LIGHTWEIGHT_PROT was 1 in the driver code. Regards #lwipWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.