2011-09-22 1:57 AM
Hi all,
I am using DfuSe demo (v3.0.0) to communicate with the board STM3220G-eval. I am willing to test, understand and confirm the leave DFU sequence. So I press the button ''Leave DFU Mode'' on the DfuSe and i can see the process happening in the progress bar upto 49% completion, but then i received an ''unexpected error'' and cant leave the DFU mode. There are no issues with communication otherwise. I am able to load the binary into the flash and verify it successfully. The problem seems to occurring consistently at 49% completion. I also tested on different computers but on all computers i receive the same ''unexpected error'' at 49%. Have anybody seen this kind of behavior earlier? My goal is simply to leave the DFU mode using DfuSe utility. Can somebody please guide me to achieve my goal? Thanks #dfuse #leave-dfu-mode-error2011-11-18 10:51 AM
I have run into the same problem - did you (or anyone) find a solution?
2011-11-19 2:29 AM
I guess the 49% is simply because it tries to do 2 things, with one progress update in between, and the first thing fails. Two main things to be done in this case are to send a zero-size download request and to poll the DFU status. Probably the ST DfuSe Demo needs to be updated to support this on STM32F2xx devices.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.