2023-10-18 12:17 AM
Hi,
I am using STM 32H745I disco boards. When I have configured the boards with LTDC interface image has been displayed on 480*272 display.
Now we have removed on board 480*272 display , we have connected external 480*480 display & I have initize the display through SPI.
I want to know wheather is it possible ?
If yes ...then how it needs to be configured ?
Thankyou
2023-10-18 6:06 AM
The datasheet of the display should tell how to use it. If it doesn't connect over LTDC, you're going to need a different interface to control it compared to the previous display.
2023-11-02 11:54 PM
so what is the question?
I understand your mean is that 1. you used LTDC to connect 480*272 display before; 2. now you want to use SPI to connect 480*480 display?
if the display support the SPI interface, it is possible to apply this display on board, but the image transfer speed will be lower than LTDC interface.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.