2015-02-28 6:07 AM
Hello, Friends!
I'm trying to generate code to work with the LAN8720 PHY + FreeRTOS through STM32Cube. I can work with ethernet, only if the PHY starts with this ethernet cable. Otherwise, the ethernet does not work.I've tried changing the PHYADR0 as 1b and 0b, without success. I've tried changing the settings of lwIP stack, also without success.I did a test with another card Waveshare using DP83848 PHY at the beginning had the same problem, but that was resolved by changing the PhyAddress 1b to 0b.* Attached are the wiring diagram of the LAN8720 plate ETHBoard of Waveshare and tabm�m the STM32Cube configuration file that I am using. #lan8720 #stm32cube #freertos2015-03-03 8:25 AM
2015-03-09 6:29 AM
Hi, Francescato!
Thanks for your answer!So I now I enabled Auto-Enabled and I imagine that when we use the lwIP and FreeRTOS stack the EthIf tasks and tcpip_thread should treat the PHY status.I keep looking at lwIP stack and in some instances the ST, a solution to this case. Any news post here.2015-03-10 12:49 AM
Ronaldo
sorry
,I do not know
lwIP
and
FreeRTOS
and I can't
help
After
a quick read
of
EthIf
I think this
can't solve
The problem is
''below
''TCP / IP stack
is related
to the
PHY
registers
lwIP
is not related
to the
PHY
(
maybe you can
install a
user callback
)tcpip_thread
assume you have
a
configured
networkbut
when the cable
is
connected
you must configure
the stack
before
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.