2020-02-04 2:57 AM
I'm launching the bootloader from within code using previously posted examples. This works fine on "Y" and DFU enumerates as expected. On rev "V" this doesn't work - no enumeration. Has the entry point changed on rev "V" or is this a bug in the bootloader which I believe is a different version in rev "V" and which other threads indicate has issues?
Is there a way of getting the bootloader entry address? SYSCFG.UR3 gives the top 16bits but where is the rest defined?
uint32_t i=0;
void (*SysMemBootJump)(void);
/* Set the address of the entry point to bootloader */
volatile uint32_t BootAddr = 0x1FF09800;
/* Disable all interrupts */
__disable_irq();
/* Disable Systick timer */
SysTick->CTRL = 0;
/* Set the clock to the default state */
HAL_RCC_DeInit();
/* Clear Interrupt Enable Register & Interrupt Pending Register */
for (i=0;i<5;i++)
{
NVIC->ICER[i]=0xFFFFFFFF;
NVIC->ICPR[i]=0xFFFFFFFF;
}
/* Re-enable all interrupts */
__enable_irq();
/* Set up the jump to booloader address + 4 */
SysMemBootJump = (void (*)(void)) (*((uint32_t *) ((BootAddr + 4))));
/* Set the main stack pointer to the bootloader stack */
__set_MSP(*(uint32_t *)BootAddr);
/* Call the function to jump to bootloader location */
SysMemBootJump();
/* Jump is done successfully */
while (1)
{
/* Code should never reach this loop */
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.