2019-06-24 9:38 PM
I have tried unsuccessfully to jump from the application area to the Boot address.
As much as I try I can not get into boot by software.
What is wrong with my code ?.
SystemInit();
HAL_RCC_DeInit();
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
__set_PRIMASK(1);
__disable_irq();
typedef void (*pFunction)(void);
pFunction Jump_To_Bootloader;
uint32_t JumpAddress;
JumpAddress = *(__IO uint32_t*) (0x1FFFF6A6 + 4);
Jump_To_Bootloader = (pFunction) JumpAddress;
__set_MSP(*(__IO uint32_t*) 0x1FFFF6A6);
Jump_To_Bootloader();
I'm using stm32F042k6k6. And every time I try to go to the boot address happens
HardFault_Handler
2023-01-21 10:43 AM
Bump.
Did you get an answer to this?
I am having the same problem with STM32F072CB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.