2021-05-06 2:54 AM
Hello all,
I am trying to implement ethernet connectivity with stm32f74 uC using lwIP stack.
I am able to generate fsdata.c file.
I have used the 3rd party tool - makefsdata.exe to generate fsdata.c file.
Now I would need another file - fsdata_custom.c before compiling the program.
Could anyone please suggest, how can I generate this file?
Also, I would like to know what is the difference between these two files.
Any help is appreciated.
2021-05-12 2:32 AM
Hello @SGupt.7 ,
Below are the steps to create the fsdata_custom.c file:
1) Make sure you have Perl installed (Google Active Perl or Strawberry Perl if you are using Windows).
2) Open a command prompt and navigate to the directory that contains makefsdata
3) Type “perl makefsdata�?.
This will overwrite your fsdata so make sure you have a backup if it contains anything you want to keep.
Check out this video, it might be useful for you.
BeST Regards,
Walid
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.