2025-08-30 5:19 AM
Hello ST Community,
I'm working on an STM32N6570-DK project where I've merged two example codes from the STM32CubeN6 repository:
1 . DCMIPP_ContinuousMode
2 . Nx_WebServer
The merged code compiles successfully in STM32CubeIDE. I've attached a ZIP file containing the full merged project for reference.
Initially, I used the linker script (STM32N6XX_AXISRAM2_fsbl.ld) , which allocates 512KB of RAM (255K + 256K) and manages Ethernet buffers, I attached .txt file named WORKING.
Camera image is visible on the LCD.
Ethernet packets (with static data) are sent at ~900 Mbps.
I need more RAM for my application. So, I modified the .ld file , i attached the txt file named NOT_WORKING
The code still compiles successfully. However, after flashing the via STM32CubeIDE:
The main problem is that , whenever i tried to modify to increase the RAM size the program starts automatically and struck in Reset Handle.
Questions :
Why does the program start executing automatically after flashing? In the original setup, it doesn't auto-run like this?
Are there specific adjustments needed for Ethernet buffers (like .tcp_sec or .nx_data) when scaling up RAM? I removed the absolute addresses, but perhaps they need remapping.
Any help or insights would be greatly appreciated!
Thanks in advance,
Solved! Go to Solution.
2025-09-02 1:53 AM
Hello @saib
To resolve these issues, you should keep the code and vector table in ROM/Flash and only expand the RAM region for data, buffers, and stack as needed. Make sure to retain the absolute addresses for the Ethernet and NetXDuo buffers and use the AT>ROM directive for the .data section to ensure proper initialization. If you need more RAM for large buffers, consider defining a dedicated section for them within the expanded RAM region, but avoid moving executable code or the vector table out of ROM/Flash.
2025-09-02 1:53 AM
Hello @saib
To resolve these issues, you should keep the code and vector table in ROM/Flash and only expand the RAM region for data, buffers, and stack as needed. Make sure to retain the absolute addresses for the Ethernet and NetXDuo buffers and use the AT>ROM directive for the .data section to ensure proper initialization. If you need more RAM for large buffers, consider defining a dedicated section for them within the expanded RAM region, but avoid moving executable code or the vector table out of ROM/Flash.
2025-09-02 4:20 AM
hello mr @Saket_Om
Yes, I have tried what you suggested. I did not move the vector table and only expanded the RAM region, as shown below:
MEMORY
{
ROM (xrw) : ORIGIN = 0x34180400, LENGTH = 255K
RAM (xrw) : ORIGIN = 0x341C0000, LENGTH = 1024K /*to 1024K to fit large buffer */
}
.large_buffer (NOLOAD) :
{
. = ABSOLUTE(0x34200000);
*(.large_buffer)
}
__attribute__((section(".large_buffer"), aligned(8)))
uint8_t large_buffer[614400];
Thanks in advance for your help!
2025-09-02 6:54 AM
Hello @saib, and welcome to ST Community!
After analyzing your project and discussing it with @Saket_Om, we found that the typical suggestion applies to other MCUs but not to STM32N6 FSBL projects. The maximum code size must not exceed 511 KB due to the bootROM size restriction, which includes a 1 KB header and authentication padding. You can refer to the articles below for more details.
To resolve your issue, you should recreate your project so that the FSBL only initializes the system and loads the main application from a separate project. This approach allows you to bypass the bootROM size limitation and thus utilize more RAM in your application.
Best regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.