2024-11-21 3:17 PM
I am having issues with my slave responding to my master. I am trying to lessen complexity by only using RXP on the slave, without TXP. The slave (Nucleo-H743ZI) responds one byte late.
On the CS interrupt I send 0 for the first byte and enable RXP.
*((__IO uint8_t *)&hspi1.Instance->TXDR) = 0;
__HAL_SPI_ENABLE_IT(&hspi1, SPI_IT_RXP);
__HAL_SPI_ENABLE(&hspi1);I then receive a byte and set the next transmit byte. I use FPint so the master does not send data when it is low (used for later implementation).
void spiISRSTM(SPI_HandleTypeDef *hspi) {
//Receive if ready
if (hspi->Instance->SR & SPI_FLAG_RXP) {
HAL_GPIO_WritePin(nFPINT_GPIO_Port, nFPINT_Pin, GPIO_PIN_RESET);
rxBuffer = (*(__IO uint8_t *)&hspi->Instance->RXDR);
(*(__IO uint8_t *)&hspi->Instance->TXDR) = 1;
HAL_GPIO_WritePin(nFPINT_GPIO_Port, nFPINT_Pin, GPIO_PIN_SET);
}
__HAL_SPI_CLEAR_UDRFLAG(hspi);
__HAL_SPI_CLEAR_OVRFLAG(hspi);
__HAL_SPI_CLEAR_EOTFLAG(hspi);
__HAL_SPI_CLEAR_FREFLAG(hspi);
}The MISO line for this setup is:
0011 1111
I would expect:
0111 1111
Any Ideas what is causing this?
Solved! Go to Solution.
2024-11-25 2:27 PM
The issue was an underrun after the first byte. Disabling and reenabling spi after read and before transmit solved the issue.
sr = hspi->Instance->SR;
if ((sr & (SPI_FLAG_RXP | SPI_FLAG_TXC)) == (SPI_FLAG_RXP | SPI_FLAG_TXC)) {
HAL_GPIO_WritePin(nFPINT_GPIO_Port, nFPINT_Pin, GPIO_PIN_RESET); //Lower nFPINT
rxBuffer = (*(__IO uint8_t *)&hspi->Instance->RXDR);
__HAL_SPI_DISABLE(&hspi1);
__HAL_SPI_ENABLE(&hspi1);
pPacketSlave->ProcessSPI();
(*(__IO uint8_t *)&hspi->Instance->TXDR) = txBuffer;
}
2024-11-22 2:26 AM
Hello @EthanMankins
Could you try activating DXP interrupt and checking on DXP flag instead of RXP?
2024-11-22 8:42 AM
Hi @Saket_Om
I have tried this and it does not make difference to the timing.
2024-11-22 2:42 PM
I have found I get an UDR Interrupt error on the second byte, not sue how this happens because the transmit is set right after each read, and the master does not send a new byte until FPInt is raised. No other bytes are UDR
2024-11-25 2:27 PM
The issue was an underrun after the first byte. Disabling and reenabling spi after read and before transmit solved the issue.
sr = hspi->Instance->SR;
if ((sr & (SPI_FLAG_RXP | SPI_FLAG_TXC)) == (SPI_FLAG_RXP | SPI_FLAG_TXC)) {
HAL_GPIO_WritePin(nFPINT_GPIO_Port, nFPINT_Pin, GPIO_PIN_RESET); //Lower nFPINT
rxBuffer = (*(__IO uint8_t *)&hspi->Instance->RXDR);
__HAL_SPI_DISABLE(&hspi1);
__HAL_SPI_ENABLE(&hspi1);
pPacketSlave->ProcessSPI();
(*(__IO uint8_t *)&hspi->Instance->TXDR) = txBuffer;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.