2017-12-03 6:51 PM
uint8_t Data_to_send[5000];
__IO uint8_t Probe=0;int main(void)
{ HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); MX_DMA_Init(); MX_USART2_UART_Init(); HAL_UART_Transmit_DMA(&huart2,Data_to_send,5000); while (1) { }}and I use two callback function :
void HAL_UART_TxHalfCpltCallback(UART_HandleTypeDef *huart)
{ Probe=1;}void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{ Probe=2;}I observe Probe variable. It never is 2. This mean is
HAL_UART_TxCpltCallback() never implement.
I don't know does this is the bug?
#stm32cube-halWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.