2019-06-13 4:49 AM
I need to know HAL library version number during device firmware build process. Is there something like __HAL_VERSION_1_9_0__ or similar defined in the HAL library code?
Thank you
Dan
2019-06-13 5:01 AM
Perhaps not ideal but
STM32Cube_FW_L4_V1.14.0\Drivers\STM32L4xx_HAL_Driver\Src\stm32l4xx_hal.c
/**
* @brief STM32L4xx HAL Driver version number
*/
#define STM32L4XX_HAL_VERSION_MAIN (0x01U) /*!< [31:24] main version */
#define STM32L4XX_HAL_VERSION_SUB1 (0x0AU) /*!< [23:16] sub1 version */
#define STM32L4XX_HAL_VERSION_SUB2 (0x00U) /*!< [15:8] sub2 version */
#define STM32L4XX_HAL_VERSION_RC (0x00U) /*!< [7:0] release candidate */
#define STM32L4XX_HAL_VERSION ((STM32L4XX_HAL_VERSION_MAIN << 24U)\
|(STM32L4XX_HAL_VERSION_SUB1 << 16U)\
|(STM32L4XX_HAL_VERSION_SUB2 << 8U)\
|(STM32L4XX_HAL_VERSION_RC))
/**
* @brief Return the HAL revision.
* @retval version : 0xXYZR (8bits for each decimal, R for RC)
*/
uint32_t HAL_GetHalVersion(void)
{
return STM32L4XX_HAL_VERSION;
}
2019-06-13 6:31 AM
Hi Clive,
Thank you for your prompt response. Why are those version macros defined in C file and not in some HAL header file.
HAL libs are not 100% compatible between various STM32 families and If I want to do conditional compilation based on HAL lib version I can't do it this way :-(.
Is there something else I can lean on?
Perhaps something to consider for the next HAL lib release.
Regards
Daniel
2020-07-31 1:38 PM
I agree with dan2, this is not very useful.
2020-07-31 1:52 PM
> Why are those version macros defined in C file and not in some HAL header file.
Because HAL is developed by brainless code monkeys...
2020-07-31 2:02 PM
As you can see, ST doesn't care! The only thing they are capable of, is randomly choosing few trivial issues and work on a fix for about a year. Anything more complex is beyond their intellectual capabilities and therefore they just ignore it...
2020-07-31 2:40 PM
Practice makes perfect. Lack of it?
2020-07-31 2:57 PM
This is the picture that come in my mind.... and I had to use a PC to push it out as on smartphone the upload button is behind the glass as the HAL version is in the C file...
2020-07-31 3:16 PM
How about the CubeIDE version in a header file?
2020-07-31 3:18 PM
.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.