STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue in sending ADC data by USB

I have a code that uses a timer to generate an interrupt every 100ms which enables the acquisition of one sample from the ADC. After the sample is obtained, it is transferred to a PC by USB. The problem is that the board gets stuck after a fixed amou...

GSant.1 by Associate II
  • 2990 Views
  • 7 replies
  • 0 kudos

https client on stm32H7 controller. I am looking if there is already code for https client that can sent REST data (like curl https://mysite.com get/post) will it be straight forward to use the stm cube with freeRTOS+LWIP+MBEDTLS ?

I though of using the NUCLEO-H743ZI(which might be an overkill) is there a demo for that ? (that I can easily open an ssl socket and send/get requests ?).1) is embed os good for this , or stm32CubeMX better ?2) Tried using the stm32f407 with freeRTOS...

Moish by Associate
  • 1023 Views
  • 0 replies
  • 0 kudos

STM32F303K8 - without CAN1 bootloader ?

Hi,regarding to AN2606 (PDF page 84 = STM32F303x4(6/8)/334xx/328xx devices bootloader), it seems that the STM32F303K8 doesn't support "CAN1 bootloader", although there's a CAN bus available. Is this a documentation failure or is this a fact?

MP.17 by Associate II
  • 1911 Views
  • 3 replies
  • 0 kudos

STM32F7 SPI interrupts stop firing with FreeRTOS

Hi, I'm using stm33F7 reading sensor via SPI communication, it's working in slave only receive mode, I can read data in interrupt mode perfectly without os, but as I enable FreeRTOS (using STM32CUBE) after a random time interrupt stops firing. I'm al...

afra by Associate
  • 805 Views
  • 0 replies
  • 0 kudos

Resolved! STM32 F407G trouble USB CDC

Hi, can somebody help with USB CDC on stm32f407G-DISC. I have configure in CUBE MX to use usb CDC in FS and when i connect to PC ( WINDOWS 10)  i see setting up device (STM32_Comport) and then pc says that USB serial device is ready to use. Why windo...

Mku1 by Associate III
  • 2472 Views
  • 5 replies
  • 0 kudos

STM32F746-DISCO audio

Hi everyoneI want use STM32F746-DISCO audio unit.I want make a application whit touchGFX which also has audio output.What are the solutions for audio output?

Timer output goes hi while starting DMA.

My CPU is STM32H750VBTxMy Configuration of the timer is void MX_TIM2_Init(void) { TIM_SlaveConfigTypeDef sSlaveConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; TIM_OC_InitTypeDef sConfigOC = {0};   htim2.Instance = TIM2; htim2.Ini...

dirk2399 by Associate
  • 1615 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.