2019-06-24 12:53 AM
I am currently starting to investigate the possibility to run the Ethercat natively (without sub processor) on an STM32F207 (running at 120 MHz) with RMII. It is supposed to be a motorcontrol application that also runns a 16 KHz control interrupt to regulate the velocity.
As I see it so far I am trying to implement two realtime applications that do not tollerate any time offset.
So simply asked: is it possible to do this (in C and not assembler)? Or is it generally done with a dedicated subprocessor.
2019-06-25 2:19 AM
EtherCat slave or master?
slave is difficult (impossible), because of the on the fly EtherCAT Communication
2019-06-25 2:44 AM
Thanks for the replie. Its a slave.
2019-06-25 3:20 AM
AFAIK, this is correct.
You would need an ASIC from Beckoff, implementing the slave access point.
2019-06-25 3:57 AM
Does anyone have experience with implementing ProfiNet directly on the STM32. It seems that it is based on standard TCP/IP.
My problem is just the 16 KHz control routine that musst run precisly and should rather not be interrupted for to long. I am not sure if this is even possible to run both the motorcontrol and the communication both in realtime on the same device. How is this generally solved? Is always a ASIC used (like the Beckhoff)?
Thanks!
2019-07-20 2:15 PM
Synchronization
PROFINET IRT uses the transparent clock mechanism to synchronize PROFINET IRT devices. The transparent clock mechanism is specified in IEEE 1588-2008 (1588 V2). This creates one control loop between the master clock and slave clocks.
STM32 ETH peripheral supports IEEE 1588-2008 and is able to output recovered clock. Although it's not a typical clock... Look for more details in reference manual. Also a timer can be connected to that clock. Most likely Your motor control clock would have to be somehow based on that clock.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.