2022-12-21 3:39 PM
We have a project on an STM32H750 using FreeRTOS and I am trying to access an I2C device after the peripheral inits but before the FreeRTOS init and scheduler start in Main.c but I get no interrupts from the I2C port. I have checked that the interrupts are enabled for the port. If I do the exact same thing in a RTOS task later it works fine. If I do I2C traffic without interrupts that works fine too so the port is working. Anyone knows why?
Solved! Go to Solution.
2022-12-21 5:01 PM
2022-12-21 5:01 PM
2022-12-22 9:03 AM
Thanks, the interrupt masking level was the only thing I didn't check yesterday. Solved it by using the
uint32_t Int_Prio = NVIC_GetPriority( ...desired interrupt... );
NVIC_SetPriority( ...desired interrupt... , Level);functions; saving the default prio levels, setting the prio level to 0, doing whatever and then restoring the prio levels.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.