2025-03-04 1:33 PM - last edited on 2025-03-04 1:53 PM by Andrew Neil
The ADC values remain unchanged even when input signals does change. The C++ code provided below should hopefully clarify the situation, as I am a stuck. Thank you in advance for any help!
#include "mbed.h"
#include "stm32l4xx_hal.h"
//Once the buffer below is filled, transfer it over to the PC
#define ADC_BUF_SIZE 1024 // Number of samples in buffer
#define SAMPLE_RATE 50000 // Sampling rate in Hz (e.g., 50 kHz)
AnalogIn adc_pin(A0); // Use A0 as the analog input pin
// ADC and DMA handles
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;
uint16_t adc_buffer[ADC_BUF_SIZE]; // ADC DMA buffer
volatile bool buffer_ready = false; // Flag to indicate data is ready
void ADC_Init() {
__HAL_RCC_ADC_CLK_ENABLE(); // Enable ADC Clock
__HAL_RCC_DMA1_CLK_ENABLE(); // Enable DMA Clock
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.ScanConvMode = DISABLE;
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = ENABLE;
hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
if (HAL_ADC_Init(&hadc1) != HAL_OK) {
printf("ADC Init Failed!\n");
}
// Configure ADC Channel
ADC_ChannelConfTypeDef sConfig = {0};
sConfig.Channel = ADC_CHANNEL_5; // Corresponds to A0
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_6CYCLES_5; // Adjust if needed
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) {
printf("ADC Channel Config Failed!\n");
}
}
void DMA_Init() {
// Configure DMA
hdma_adc1.Instance = DMA1_Channel1;
hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;
hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
hdma_adc1.Init.Mode = DMA_CIRCULAR;
hdma_adc1.Init.Priority = DMA_PRIORITY_HIGH;
if (HAL_DMA_Init(&hdma_adc1) != HAL_OK) {
printf("DMA Init Failed!\n");
}
__HAL_LINKDMA(&hadc1, DMA_Handle, hdma_adc1);
// Enable Interrupt on DMA Transfer Complete
HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
}
void Start_ADC_DMA() {
HAL_ADC_Start_DMA(&hadc1, (uint32_t*)adc_buffer, ADC_BUF_SIZE);
printf("ADC Sampling Started...\n");
}
extern "C" void DMA1_Channel1_IRQHandler() {
HAL_DMA_IRQHandler(&hdma_adc1);
}
// Callback function when buffer is full
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc) {
if (hadc->Instance == ADC1) {
buffer_ready = true; // Signal that buffer is full
}
}
void Process_ADC_Data() {
if (buffer_ready) {
buffer_ready = false;
for (int i = 0; i < ADC_BUF_SIZE; i++) {
printf("Sample %d: %d\n", i, adc_buffer[i]);
}
}
}
int main() {
printf("Starting ADC DMA Sampling...\n");
ADC_Init(); //
DMA_Init(); //Direct memory access - giving permission to ADC to write into the memory
Start_ADC_DMA(); //Start DMA writing
while (1) {
Process_ADC_Data();
ThisThread::sleep_for(10ms); // Avoid CPU overload
}
}
Code formatting applied - please see How to insert source code for future reference.
2025-03-05 12:35 AM
Hello @mbe
Could you check with ADC calibration before starting the conversion please?
/* Run the ADC calibration in single-ended mode */
if (HAL_ADCEx_Calibration_Start(&AdcHandle, ADC_SINGLE_ENDED) != HAL_OK)
{
/* Calibration Error */
Error_Handler();
}
/*##-3- Start the conversion process #######################################*/
if (HAL_ADC_Start_DMA(&AdcHandle) != HAL_OK)
{
/* Start Conversation Error */
Error_Handler();
}
2025-03-05 12:38 AM
@mbe wrote:The ADC values remain unchanged even when input signals does change.
Please give details of the input signal, and how it's connected.
Are you sure that the input signal is actually reaching the correct pin on the chip package?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.