2020-02-07 2:57 PM
@STM32H743_User @STM32F103 because both interface are different as shown below and also its physical layer (PHY) is different.
2020-02-08 7:28 AM
Code as an image, some nonsense users mentioned as "MCUs" and no information for an actual platform...
If the question is about lwIP, then yes - it supports working with multiple physical interfaces of different types simultaneously. In a normal IP stack typically UDP/TCP connection is bound to IP address and port, not a specific physical interface. And lwIP supports binding connection to either a single IP address or any IP address.
2020-02-08 9:45 AM
If your code supports it, yes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.