2020-06-12 1:43 PM
I am using the stm32H743 and have added USB OTG FS and FatFS to my project.
A function is generated in Main() : static void MX_TIM8_Init(void)
and the last thing this function calls is: HAL_TIM_MspPostInit(&htim8);
But this file is NOT generated. Why ?
2020-06-12 5:52 PM
Are you sure? I just generated a project like that and it generated fine for me. The function is in stm32h7xx_hal_msp.c.
void HAL_TIM_MspPostInit(TIM_HandleTypeDef* htim)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(htim->Instance==TIM8)
{
/* USER CODE BEGIN TIM8_MspPostInit 0 */
/* USER CODE END TIM8_MspPostInit 0 */
__HAL_RCC_GPIOC_CLK_ENABLE();
/**TIM8 GPIO Configuration
PC6 ------> TIM8_CH1
*/
GPIO_InitStruct.Pin = GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF3_TIM8;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/* USER CODE BEGIN TIM8_MspPostInit 1 */
/* USER CODE END TIM8_MspPostInit 1 */
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.