cancel
Showing results for 
Search instead for 
Did you mean: 

I am using the Nucleo-h745ziq board.Board interface with User usb port as custome HID.Through USB I am sending and receving the data.For this I am using the USB HID Demonstartor (v1.0.2).

MDeva.1
Associate II

I am able to send the data but unable to receive from USB HID Demonstrator.

Here is my code:

uint8_t USBD_CUSTOM_HID_ReceivePacket(USBD_HandleTypeDef *pdev)

{

 USBD_CUSTOM_HID_HandleTypeDef *hhid;

 if (pdev->pClassData == NULL)

 {

  return (uint8_t)USBD_FAIL;

 }

 hhid = (USBD_CUSTOM_HID_HandleTypeDef *)pdev->pClassData;

 /* Resume USB Out process */

 (void)USBD_LL_PrepareReceive(pdev, CUSTOM_HID_EPOUT_ADDR, hhid->Report_buf,

                USBD_CUSTOMHID_OUTREPORT_BUF_SIZE);

 for(uint8_t i=0;i<1;i++)

  {

  rx_data[i]=hhid->Report_buf[i];

  }

if(rx_data[0]==1) HAL_GPIO_TogglePin(GPIOE, GPIO_PIN_1);

if(rx_data[0]==2)  HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_14);

 return (uint8_t)USBD_OK;

}

__ALIGN_BEGIN static uint8_t CUSTOM_HID_ReportDesc_FS[USBD_CUSTOM_HID_REPORT_DESC_SIZE] __ALIGN_END =

{/* USER CODE BEGIN 0 */

0x06, 0x00, 0xFF,  // Usage Page = 0xFF00 (Vendor Defined Page 1)

 0x09, 0x01,     // Usage (Vendor Usage 1)

 0xA1, 0x01,     // Collection (Application)

 // Input report

 0x19, 0x01,     // Usage Minimum

 0x29, 0x40,     // Usage Maximum

 0x15, 0x80,//0x00,  // Logical Minimum (data bytes in the report may have minimum value = 0x00)

 //0x26, 0xFF, 0x00, // Logical Maximum (data bytes in the report may have maximum value = 0x00FF = unsigned 255)

 0x25,0x7f,

0x75, 0x08,       // Report Size: 8-bit field size

 0x95, CUSTOM_HID_EPIN_SIZE,// Report Count

 0x81, 0x02,       // Input (Data, Array, Abs)

 // Output report

 0x19, 0x01,       // Usage Minimum

 0x29, 0x40,       // Usage Maximum

 0x75, 0x08,       // Report Size: 8-bit field size

 0x95, CUSTOM_HID_EPOUT_SIZE,// Report Count

 0x91, 0x02,       // Output (Data, Array, Abs)

 0xC0

 /* USER CODE END 0 */

  /*   END_COLLECTION        */

};

#ifndef CUSTOM_HID_EPIN_SIZE

#define CUSTOM_HID_EPIN_SIZE             0x20U

#endif

#define CUSTOM_HID_EPOUT_ADDR            0x01U

#ifndef CUSTOM_HID_EPOUT_SIZE

#define CUSTOM_HID_EPOUT_SIZE            0x20U

#endif

Here is I setup done.I am unable to receive data .I forgot to intilasation the parameter or I am using wrong terminal? Because I am using USB Custome HID inerface.Can someone Help me?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hello @MDeva.1​ ,

You can refer to following example available under STM32CubeH7 package (path: Projects\STM32H743I-EVAL\Applications\USB_Device\CustomHID_Standalone ).

You could use this as inspiration.

BeST Regards,

Walid

View solution in original post

1 REPLY 1

Hello @MDeva.1​ ,

You can refer to following example available under STM32CubeH7 package (path: Projects\STM32H743I-EVAL\Applications\USB_Device\CustomHID_Standalone ).

You could use this as inspiration.

BeST Regards,

Walid

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.