2020-09-01 1:54 PM
Hi,
I'm trying to implement a webpage to change network parameters (IP, Gateway, netmask) on nucleo-F429ZI
If i change parameters before httpd_init() is called, all works ok: the board responds to the ping, and the httpd returns the webpages. But if I call httpd_init(), and after I change network parameters, the network interface responds to ping on the new address until I try to request a webpage. When I request a webpage, httpd go to timeout and the board not respondig to ping.
this is the code to change network parameters:
netif_set_down( &gnetif );
IP4_ADDR(&ipaddr, IP_ADDRESS[0], IP_ADDRESS[1], IP_ADDRESS[2], IP_ADDRESS[3]);
IP4_ADDR(&netmask, NETMASK_ADDRESS[0], NETMASK_ADDRESS[1] , NETMASK_ADDRESS[2], NETMASK_ADDRESS[3]);
IP4_ADDR(&gw, GATEWAY_ADDRESS[0], GATEWAY_ADDRESS[1], GATEWAY_ADDRESS[2], GATEWAY_ADDRESS[3]);
netif_set_addr(&gnetif,&ipaddr,&netmask,&gw);
if (netif_is_link_up(&gnetif))
{
netif_set_up(&gnetif);
}
else
{
netif_set_down(&gnetif);
}
thank you
2020-11-23 11:27 PM
Hi, I think you might be overdoing it. Ip address change does not need so much configuration when done after the interface has been initialized.
I am using the following function to do it after initialization by cubemx generated code. I have this function inside lwip.c so that gnetif is available there as global. You can put this inside /* USER CODE BEGIN 2 */ on the top, so it's safe to regenerate.
/** Set new ip address to ethernet
* @param addr is the new ip address as a string, eg 192.168.1.1
* @param netmask is the new netmask address as a string, eg 255.255.255.0
*/
void setIpAddr(char* addr, char* netmask)
{
ip4_addr_t newip, newMask;
if (ip4addr_aton(addr, &newip))
{
netif_set_ipaddr(&gnetif, &newip);
}
if (ip4addr_aton(netmask, &newMask))
{
netif_set_netmask(&gnetif, &newMask);
}
}
More details in lwip docs:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.