2024-05-30 7:35 AM - edited 2024-05-30 7:44 AM
Hello,
I am new to STM32 and I am trying to write into FLASH memory using some reference code I found in internet. Here is my write function:
uint32_t Flash_Write_Data (uint32_t StartPageAddress, uint32_t *Data, uint16_t numberofwords)
{
static FLASH_EraseInitTypeDef EraseInitStruct;
uint32_t PAGEError;
int sofar=0;
/* Unlock the Flash to enable the flash control register access *************/
HAL_FLASH_Unlock();
/* Erase the user Flash area*/
uint32_t StartPage = GetPage(StartPageAddress);
uint32_t EndPageAdress = StartPageAddress + numberofwords*32;
uint32_t EndPage = GetPage(EndPageAdress);
/* Fill EraseInit structure*/
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.Page = page_indx;
EraseInitStruct.NbPages = ((EndPage - StartPage)/FLASH_PAGE_SIZE) +1;
if (HAL_FLASHEx_Erase(&EraseInitStruct, &PAGEError) != HAL_OK)
{
/*Error occurred while page erase.*/
return HAL_FLASH_GetError ();
}
/* Program the user Flash area word by word*/
while (sofar<numberofwords)
{
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_QUADWORD, StartPageAddress, Data[sofar]) == HAL_OK)
{
StartPageAddress += 32; // use StartPageAddress += 2 for half word and 8 for double word
sofar++;
}
else
{
/* Error occurred while writing data in Flash memory*/
return HAL_FLASH_GetError ();
}
}
/* Lock the Flash to disable the flash control register access (recommended
to protect the FLASH memory against possible unwanted operation) *********/
HAL_FLASH_Lock();
return 0;
}
-----------------------
Function call for write in main.c:
char *data = "hello stm32";
uint32_t Rx_Data[30];
Flash_Write_Data(0x083FE000 , (uint32_t *)data, 2);
float number = 123;
Flash_Write_NUM(0x083FC000, number);
-----------------------
When I tried to write the data into flash memory my application just writes 0's in the memory (I checked using STM32 programmer)
and when I tried to write a number into the flash instead of char data, I get hardfault handler issue.
What am I doing wrong here? Can anyone shed some light please?
Regards
RiverDI user
Solved! Go to Solution.
2024-06-24 9:17 PM
can you find the '\Projects\STM32U5x9J-DK\Examples\FLASH\FLASH_EraseProgram\...'?
2024-06-02 11:31 PM
which MCU are you used? since your write flash address is start from the internal 0x083FE000, your MCU flash size is bigger than 3M?
2024-06-24 2:14 AM
Hello,
Yes, my Flash is 4 MB and which has 512 pages of 8KB each.
My MCU is: STM32U5A9
I am trying to write into flash using my above code, after I write into flash I am getting hard fault handler error. Once I restart the device, I could see the data written into the flash, but my problem is my app is getting into "hard-fault" handler when I write into flash.
Could you point out what is missing in my code?
Thanks & Regards
2024-06-24 2:59 AM - edited 2024-06-24 3:00 AM
there is no obvious problem for your code, but there are some rules to write flash, like flash write align 4 bytes, flash latency configuration must correct.... I suggest you to download 'STM32CubeMX' tool to execute the flash operate demo to find the cause.
STM32CubeMX link: https://www.st.com/en/development-tools/stm32cubemx.html#get-software
2024-06-24 3:18 AM
Hello, Can you point out the example flash operate demo name? I couldn't find it in my IDE example projects.
2024-06-24 9:17 PM
can you find the '\Projects\STM32U5x9J-DK\Examples\FLASH\FLASH_EraseProgram\...'?
2024-08-18 11:46 PM
Hello EXUE.2,
I was able to write the data into FLASH by using the reference example you have shared. Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.