2018-06-18 12:47 PM
Hello everybody,
I want to read ADC data from 2 channels using stm32L011 microcontroller. I can successfully read in 'int main ()' by calling the HAL_ADC_Start_DMA function. However, I want to read the adc data for a certain period of time in the 'HAL_LPTIM_AutoReloadMatchCallback' function and then turn off the adc.
In summary, when LPTIM performs an automatic upload, I want to read the adc data from both channels and then turn off the adc. When I read data from two channels using DMA, there is a problem with the timer and I can not turn off the ADC. The program is not working properly.
Any suggestions?
#stm32l011k4 #dma #hal-adcWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.