2024-01-05 11:07 PM
Hi,
I’m using the latest X-CUBECELLULAR version v7.1.0 on the BL462E-CELL1.
However, the modem factory FW version (RK_03_00_00_00_11851_001) isn’t compliant with the X-CUBECELLULAR v7.1.0.
From the release notes, the X-CUBECELLULAR v7.1.0 requires RK_03_00_00_00_04121_001.
However, I don’t know how and where to download the RK_03_00_00_00_04121_001 modem firmware version.
Your help is much appreciated.
Kind regards.
Solved! Go to Solution.
2024-02-12 8:17 AM
After contacting support from muRata, I was told the modem factory FW version (RK_03_00_00_00_11851_001) is a newer version compared to RK_03_00_00_00_04121_001. So, the “RK_03_00_00_00_11851_001” version works well with the X-CUBECELLULAR version v7.1.0.
I have tested it, and works perfectly.
Regards.
2024-02-12 8:17 AM
After contacting support from muRata, I was told the modem factory FW version (RK_03_00_00_00_11851_001) is a newer version compared to RK_03_00_00_00_04121_001. So, the “RK_03_00_00_00_11851_001” version works well with the X-CUBECELLULAR version v7.1.0.
I have tested it, and works perfectly.
Regards.
2024-02-12 8:21 AM
To download the RK_03_00_00_00_04121_001 modem firmware for your BL462E-CELL1 with X-CUBECELLULAR v7.1.0:
1. Check the official website of the device manufacturer for a downloads or support section.
2. Contact customer support for assistance.
3. Refer to the device's documentation or user manual.
4. Check developer community forums for relevant information.
5. Explore any proprietary update tools provided with the device.
Download firmware from official and trusted sources to ensure compatibility and security. If issues persist, contact the device manufacturer's technical support.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.