2020-03-22 5:01 PM
Hi everybody,
I've been trying for a while to read multiple bytes from an LIS3MDL accelerometer. I know how to read and write registers but one at a time. I can't figure it out the multiple part...
So, if I want to read from reg 0x27 to 0x2D, I understand that I need to set bit0 to 1 (for read operation) and MS bit to 1 (for multiple read). Then :
TxMagOut[0] = 0x27|0xC0;and
RxMagOut[8] = {0}; // initialisationI use transmiReceive with TxMagOut. I said that my data is 8 bytes so it know when to stop reading (at 0x2D)
HAL_SPI_TransmitReceive(&hspi3,TxMagOut ,RxMagOut , 8, 100);I should get my data in RxMagOut from [1] to [8]. Right? At least this is my best idea.
Am I doing something wrong? Do someone see an error there?
If there is a simple example with HAL of multiple byte read that you know of ? I would be gratefull.
Thanks! :)
2020-07-25 8:00 AM
AFAIK HAL_SPI_TransmitReceive(&hspi3,TxMagOut ,RxMagOut , 8, 100);
"8" here is number of tx bytes, not the rx bytes as you assumed.
2020-08-03 1:58 PM
Hi @JMart.5, did you end up solving the issue? I have the same problem too.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.