2022-01-02 7:57 AM
Hallo,
I can't find any info about this theme!
Can someone please help me with some hints on how to "connect" FATFS as filesystem driver with the SDMMC1 interface (in 4 bits mode) as hardware.
Many Thanks in advance,
Michael
Solved! Go to Solution.
2022-01-03 1:23 AM
In that case you can refer to the example provided in STM32CubeH7 under the path Projects\STM32H743I-EVAL\Applications\FatFs\FatFs_uSD_Standalone
2022-01-03 12:43 AM
Hello @Mick P. F. ,
Please refer to this video (from t= 2:03) on YouTube done for F7, normally it would be the same steps: link.
Hope this will help you.
2022-01-03 1:15 AM
Hello SofLit,
I have found some projects and examples on this topic, but they all relate to the STM32F MCUs.
There are two problem with this: When I activate FATFS in STM32CubeMX, I can only select the "User defined" mode but not "SD Card". In addition, SDMMC1 of the H7 is not DMA capable inside STM32CubeMX (in contrast to STM32F).
I have now decided to access the SD card via SPI because it is easier and I only want to read a little couple of data.
Thanks for your help.
2022-01-03 1:23 AM
In that case you can refer to the example provided in STM32CubeH7 under the path Projects\STM32H743I-EVAL\Applications\FatFs\FatFs_uSD_Standalone
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.