2025-01-02 4:07 AM
Hii, I have been trying to interface Nucleo-H503 with SD card adapter which has SPI pins to interface, in stm32cubeide i selected SPI1 and FileX in the middleware. But unable to get how to write code for it for creating file and saving Helloworld in the file created in SD card.
2025-01-02 4:36 AM
Hello @Shubham08
I suggest you follow this wiki that should be really helpful for you.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-03 4:23 AM
Sir, i have gone through the Wiki and also gone through the chapter link in the Github but didn't get solution. That is I have 32GB memory card normally available in market, i have microsd card module which have SPI interface, and Nucleo-H503 board.
In the STM32CubeIDE, there is no option of SDIO and SDMMC so I have selected SPI interface and in the middleware there was no FATS instead of that there was FileX and ThreadX . I tried to get to know how to use FileX, for datalogging using microsd card as in the github and wiki there the syntax and method for SRAM is given. Means i am not getting about the folder stucture where to add the appropriate coding part so that i can do the datalogging using microsdcard using FileX as it is new to me. That is i need the help what lines of code to be added in main.c or fileX for getting started with datalogging usign microSD card.
Sorry for the basic question but i am not getting about how to implement it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.