2024-12-02 7:01 PM - last edited on 2024-12-09 7:14 AM by mƎALLEm
I am using a user defined diskio function (found online here https://github.com/kiwih/cubeide-sd-card/tree/master/cubeide-sd-card/FATFS/Target) for doing read and writes using SPI2. I am trying to read 50,000 floats from a file that containsway more than that. My SPI baudrate is setup at 48 Mbits/s(SPI clock at 96 with prescalar divided by 2) and attaching the spi signals to a oscilloscope does show that the clock speed and the data speed is correct. However,
f_read(&file, arr_floats, 50000* 4, &bytesread);
takes over 7 seconds to read all the bytes when at 48Mhz it should be reading it in way less than a second. I am using a LEXAR 32gb V10 sdcard in FAT32 format, and was wondering what I could do to increase the read speed of the floats???
I have tried several different methods to improve it: reading 512 bytes at a time instead of the 50,000 * 4 at a time, I have tried to implement the dma, I have tried to use a different SDcard, but none of the things helped in increasing the speed by much.
Any help will be much appreciated. Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.