2020-10-06 7:02 PM
If we want to implement USB to multi-interface at the same times
USB to UART1~3
USB to I2C1~3
USB to SPI
USB to PWM
USB to SD card
We use STM32F4 , USB 2.0 have 5 in / 5 out endpoints
i think we could use USB mass storage protocol to implement USB to SD
but the remain endpoints is not enough to implement standard USB protocol such as USB to UART1~4 (CDC),
What kind of method could i use to implement usb to other interface?
i do some research
USB HID
Self define descriptor use report ID to distinguish interface(UART/I2C/PWM...)
USB CDC
Use virtual com to send self-defined command to communicate (UART/I2C/PWM)
....
Which is better use in Linux? or is there another method for USB to multi-interface ?
Is there any related sample code could reference?
Thanks alot
2020-10-07 12:04 AM
Options are:
- use the CDC class and select ab different mcu with more endpoints (but it sounds you want more channels than might be endpoints available in any STM32)
- use one CDC class and encapsulate data for several channels into your protocol, multiplexing/demultiplexing at the application level (this sounds to be the most plausible solution)
- do the same at system level, i.e. develop your own non-class USB Interface, and write corresponding driver at the host side i.e. linux, performing basically the same multiplexing/demultiplexing, presenting it to application(s) as separate streams
Definitive not something you can get ready made with examples.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.