2021-10-20 9:32 PM
Hi,
I am working to make application of USB host. At initial stage, I need to read how big is the free size of attached USB stick using the FAT file system middle ware. Can someone give me some pointer which FAT system interface I can use? I know how to mount and dismount, but not sure how to get this USB stick free size.
Solved! Go to Solution.
2021-10-20 10:49 PM
2021-10-20 10:49 PM
2021-10-21 3:15 AM
void printsize(uint32_t size, char *s)
{
if (size >= 1000000) // Storage vendor math
printf(" %6.1lf GB %s\n", (double)size / 1000000.0, s);
else if (size >= 1000)
printf(" %6.1lf MB %s\n", (double)size / 1000.0, s);
else
printf(" %6.1lf KB %s\n", (double)size, s);
}
{
FATFS *fs;
DWORD fre_clust, fre_sect, tot_sect;
/* Get volume information and free clusters of drive 1 */
res = f_getfree("", &fre_clust, &fs);
if (res != FR_OK)
{
#ifdef DBG
printf("res = %d f_getfree\n", res);
#endif
return;
}
switch(fs->fs_type)
{
case FS_FAT12 : puts("FAT12"); break;
case FS_FAT16 : puts("FAT16"); break;
case FS_FAT32 : puts("FAT32"); break;
case FS_EXFAT : puts("EXFAT"); break;
default : puts("Unknown FAT");
}
/* Get total sectors and free sectors */
tot_sect = (fs->n_fatent - 2) * fs->csize;
fre_sect = fre_clust * fs->csize;
/* Print the free space (assuming 512 bytes/sector) */
printsize(tot_sect / 2, "total drive space");
printsize(fre_sect / 2, "available");
printsize((tot_sect - fre_sect) / 2, "used");
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.