2022-01-10 1:41 AM
I’m working with a NUCLEO-H723ZG
I can generate a cube project with the ADC & DMA features working the way I want them to, but when I import the necessary code snippets into the LWIP TCP echo demo project & run on the same hardware the DMA fails on the first IRQ with a transmit error.
looking over the registers in the debugger both ADC & DMA seem to have the right contents regarding configuration.
any idea why the DMA would encounter a transmit error?
anyone with any experience of adding stuff to the LWIP tcp echo project?
2022-01-12 6:38 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.