2021-02-24 10:33 AM
Helllo,
I'm trying to communicate with USB module that exposes 3 virtual com ports if used under PC and Windows. It's AT command set based communication module.
I'd like to connect to it over USB Host library on STM32F779.
I have basic code running, module is properly powered, Appli_state changes to APPLICATION_START state.
Now I wonder what should I do next? I guess I need to enumerate virtual com ports
and connect to the proper one.
How do I do this? I have read USB Host library document but it's only general.
Is there any working example - possibly with FreeRTOS ?
Thanks,
regards.
2021-02-24 12:15 PM
> I guess I need to enumerate virtual com ports
It looks like a composite device with 3 interfaces. So yes, parse the descriptors and find the needed function (or you need all 3?)
From the interface descriptor find the endpoint descriptors. Then use these endpoints as in CDC host example.
-- pa
2021-02-24 12:25 PM
Hello,
thanks for info... Can you please help me with functions that will do this ?
Are descriptors already in there or should I call functions ? Is USBH_ReEnumerate the right to do the enumeration ?
Any hint or pointer to more info how to parse descriptors and find the correct one ?
Thanks,
2021-02-25 11:53 PM
Hello,
I've got few steps further, I can now detect device and I see this on console :
USB Device Reset Completed
PID: 296h
VID: 2c7ch
Address (#1) assigned.
Manufacturer : Qualcomm, Incorporated
Product : Qualcomm CDMA Technologies MSM
Serial Number : b349f9e4
Enumeration done.
This device has only 1 configuration.
Default configuration set.
Device remote wakeup enabled
DEBUG : Cannot Find the interface for Communication Interface Class.
CDC class started.This is a BG96 module called "LTE IOT Click 2" from Mikroelektronika and it seems that it doesn't implement VCOM under CDC class,
but it reports as 0xff class...
Any advice whether it is possible to connect to those devices (maybe FTDI are similar) ?
Under Windows I had to install custom drivers to get it recognized and working...
Thanks...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.