2022-11-28 1:48 AM
Hi Team,
I am looking for the help to configure my STM32 MCU as Composite Device (MSC + CDC). I have gone through multiple blogs and examples available in ST community but none of the example shown me how to configure USB as Composite class (CDC + USB).
I am using STM32F750x8 could you please help me on this by sharing some inputs?
2022-11-28 9:33 AM
Look at the STM32 USB code. After a week or so of heavy analysis, you will probably be able to understand their composite device support (it's already there, just not officially supported by CubeMX). Or maybe spend 3 days on writing your own USB stack, designed for composite from the ground up. As a side effect you should be able to save like 80% of required Flash and RAM size. That's what I did - 2 VCOMs + printer take 3.5 KiB of Flash + 300 B of RAM. MSC should add no more than 1.5 KiB - I will add it soon.
2023-05-23 2:29 AM
Hi! Is it possible to share your example or at least a glimpse of it? Thank you
2024-01-18 10:23 PM
Hi,
it is a shame that CubeMX does not support a combination of several device classes. After one day of searching examples i found a "software pack" for CubeMX:
alambe94/I-CUBE-USBD-Composite: Create STM32 USB Composite devices with ease. (github.com)
ST, please support this project and promote it, so we all can save lifetime!
I use:
CubeMX 6.10.0
CubeIDE 1.14.0
Processor: STM32F407VGT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.