2021-08-07 11:44 PM
I'm using STM32F415VG, on which we built uc-osIII, I've built a Fatfs on nand flash, unfortunately, we had to use a block at the end of low-level nand flash read and write. How can I change the size of Fatfs and realize that this low-level function coexists with the file system at the same time, can I realize it?
2021-08-08 8:03 AM
The large erase block size of NAND memories is ill-suited to MCU with limited RAM resources.
Do you have to use FatFS? Could you use something more incremental / journalling ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.