2024-11-10 5:10 PM
I want to implement a firmware upgrade feature. Currently, I am doing it as follows: on the M4 core, I have a bootloader and an application; on the M7 core, there is also a bootloader and an application. The M4 application is located at address 0x08120000, and the M7 application is located at address 0x08020000. I’m not sure if this approach is feasible or if there is a recommended upgrade method. Currently, the jump between the cores does not succeed, and I don’t know why. Are there any specific considerations when performing a jump between dual-core firmwares?
Solved! Go to Solution.
2024-11-11 1:17 AM
Hello @yue9035 and welcome to the community,
You can inspire from this example from Github: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H743I-EVAL/Applications/IAP
2024-11-10 5:22 PM - last edited on 2024-11-14 3:42 AM by mƎALLEm
I use the following code to jump to the M7 application, and similarly, after changing the address, I use the same method to jump to the M4 application.
#define APPLICATION_M7_ADDRESS 0x08020000
void JumpToApplication(void)
{
__disable_irq();
ApplicationEntry = (pFunction) (*(__IO uint32_t*) (APPLICATION_M7_ADDRESS + 4));
uint32_t appStack = *(__IO uint32_t*) APPLICATION_M7_ADDRESS;
__set_MSP(*(__IO uint32_t*) APPLICATION_M7_ADDRESS);
ApplicationEntry();
}
In the M7 application, I used SCB->VTOR = 0x08020000 to set the interrupt vector offset address. Similarly, in the M4 application, I used SCB->VTOR = 0x08120000 to set the interrupt vector offset address.
2024-11-11 1:17 AM
Hello @yue9035 and welcome to the community,
You can inspire from this example from Github: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H743I-EVAL/Applications/IAP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.