2017-01-22 6:53 PM
I am using the FUSB2805 HS USB phy with the STM32469. The usb interface seems to be working alright. Sometimes the phy gets into a weird state after restarting the micro but not the phy. I would like to perform a soft reset on the phy by setting bit 5 of the phy control register high.
The problem is I can't figure out the best way to send this command. I am using the HAL library which has quite a few different layers of abstraction.
Does anyone have any experience doing this or where I should be doing this?
Currently, to send data the layers look like this:
CDC_Transmit_HS > USBD_CDC_TransmitPacket > USBD_LL_Transmit > HAL_PCD_EP_Transmit > USB_EP0StartXfer > Registers
#external-phy #usb #usb-hs #ulpiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.