2023-03-16 5:36 AM
I am trying to send some communication from an Nucleo-F412ZG board over USB. I am currently using CDC_Transmit_FS function but this seems to only send char values and I would like to be able to send an uint8_t variable and have it come out as a meaningful set of characters, is there a way to do this with the CDC_Transmit_FS function or do I need to use something else?
2023-03-16 6:58 AM
You'd need to create the ASCII or human readable forms with sprintf() or itoa() into character strings,and then cast those into (uint8_t *) collections of bytes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.