2021-12-01 7:21 AM
2021-12-01 10:59 AM
And if the buzzer is disconnected, but still handled in software?
If this removes the problem, the buzzer probably generates too much interference, or you are overloading the mcu pin. In other words, in this case it's a hardware problem.
JW
2021-12-01 11:34 PM
Good morning jan,
thank's for answer. If I use the code without active buzzer (speaker 6Ohm on an class d amplifier and amplifier (SSM2305RMZ-R2) not activated) there's no problem. I think, it's a hardware problem, but is it possible to see in software that there is a problem. If so I can reinitiate the hardware.
best regards
Josef
2021-12-01 11:59 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.