STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Running C functions transfered during runtime

Hi,I'm currently developing a PLC-like device based on a STM32F429ZI. It works with FreeRTOS, and the I/O logic is implemented in a single C function, which only accesses a couple of buffers (the locations of which are known prior to compilation). Th...

Áde R.1 by Associate II
  • 3713 Views
  • 4 replies
  • 0 kudos

STM32F746 USB MSC Host not working

I am using STM32F746G-DISCO board.Configured USB FS in MSC HOST mode.After connecting the Pendrive, ReqStatus in following part returns USBH_BUSY  case ENUM_IDLE:   /* Get Device Desc for only 1st 8 bytes : To get EP0 MaxPacketSize */   ReqStatus = U...

Rohit.1 by Associate II
  • 1300 Views
  • 1 replies
  • 0 kudos

FATFS on external SDRAM Problem

HiI work on stm32f746 discovery and I want to configure FATFS on external sdram. I use STM32CubeIDE 1.6.1. when I create my project and mount disk, return error (value 13 = FR_NO_FILESYSTEM). does everyone know about this problem or is there any samp...

EKari.2 by Associate II
  • 1602 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H745II, SPI Boot programming not working.

Hi .I have STM32H745II controller, I am keeping its boot pin at HIGH state and providing reset condition.Host controller's SPI pins are connected to SPI3 pins PC10, PC11, PC12 and PA15 of STM32H745II for communicating in SPI boot mode.Here STM32H745I...

VTaya.1 by Associate III
  • 3310 Views
  • 5 replies
  • 0 kudos

How to abort or timeout CDC_Transmit_FS

I am sending with CDC_Transmit_FS by USB CDC, but USB_TransmitCplt_Callback is not called unless the other computer receives it on the COM port.How do I time out or abort a send?MCU: STM32L433CCUxLibrary Version: STM Cube FW_L4 V1.17.0

Yoshi1 by Associate III
  • 3066 Views
  • 4 replies
  • 1 kudos

STM32G0 USB_DP/DM 3.3Volt

we are planning to use STM32G0 for our next generation design with its USB port, two application is considered:Use it as VCP, the signal from PC is +5 Volt, but the MCU is +3.3 Volt, can the USB port DP/DM pin directly connect to MCU pins? or require...

STM32F769 ethernet chip power up issue

Hello,This is nur. I need your help. I am working on STM32F769 phy chip , RMII interface. Once I apply power the stm chip then Ethernet cable clicked , there is no connection. if Ethernet cable does not click into place before power is applied to the...

nur by Associate II
  • 1587 Views
  • 2 replies
  • 0 kudos

Corrupted ETH Rx Buffer in STM32H7

Hello everyone,I'm running a webserver on a STM32H7. Code was generated with CubeIDE 1.5.0, using LwIP V2.1.2 and the Firmware-Package V1.8.0. So far, I had no problems receiving or transmitting smaller files, in the x-xx kB range from the MCU to a c...

_legacyfs_online_stmicro_images_0693W00000BaNHa.png _legacyfs_online_stmicro_images_0693W00000BaNGm.png _legacyfs_online_stmicro_images_0693W00000BaNMH.png _legacyfs_online_stmicro_images_0693W00000BaNOl.png
DWeb_2 by Associate III
  • 4243 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.