2021-12-20 9:35 PM
2022-01-11 7:25 AM
Hi @p123,
The X-CUBE-SAFEA1 provides code example that can be ported on other HW platform.
On the STM32G484E-EVL, there is no Ardunio connector, therefore you will need to use jumper wire on CN2 for instance.
Then you will need to customize the stsafea_service_interface.c file to map on the I2C3 for the I2C_Send and I2C_Received.
For the mbedtls porting, do not forget to use the config_mbedtls.h from the Inc directory of the example you are porting.
Best Regards,
Benjamin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.