2023-08-15 11:11 AM
Hi - I am new to the STM32CubeIDE - moving from Attolic.
I have created a new STM32 project using STM32CubeIDE 1.9.0 for a STM32L151VET6 using New Project.
Our board is built to use an internal oscillator.
I can try to debug the basically empty new created project or add just a for loop in the while(1) in main() and either way it immediately stops on Hardfault_Handler.
In the Fault Analyzer :
X Bus, memory management or usage fault (FORCED)
X Imprecise data access violation (IMPRECISER)
X Stacking error (STKERR)
I have set a breakpoint on the while(1) and on the for loop inside it and neither are ever hit.
I believe I have set the pins in the IOC to match my board ( UART, SPI, GPIO )
Any suggestions on how to proceed ?
Thanks!
Solved! Go to Solution.
2023-08-16 1:29 PM
Thanks!!
I found it right away looking at the startup files. Realized the board I am using has a STM32L151V C T6, and I had selected a V E T6 because that is on another board on my desk - we use both in production.
Thanks for you guys help !
2024-11-27 2:15 AM
Thank you so much for posting your solution. I was fighting with my (first) custom board for the same reason you're describing: no code was executing at all, seemed to crash before break points even trigger, and looking in the SFRs (while debugging, upper right hand corner) under Cortex M4 -> Control -> CFSR I was seeing both STKERR and IMPRECISERR set.
Turns out, I wrote my code originally on a Nucleo featuring the STM32F401R E T6, but my board uses the STM32F401R C T6. I made a new project with the correct chip and it immediately worked. Thanks again!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.