cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_SPI_Abort() malfunction (from STM32f7xx_hal_spi)

kluszkiewicz
Associate

I'm trying to use HAL_SPI_Abort() os SPI2 interface in DMA mode for STM32F769NI MCU and program hangs in it in loop:

 while (hspi->State != HAL_SPI_STATE_ABORT)

So it seams that State should be changed in interrupts, I think that in SPI2_IRQn interrupt, which is not trigerred in DMA mode.

Could you please advice.

BR,

Krystian

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
kluszkiewicz
Associate

Issue is still not resolved on my side - please advice.

I'm including my SPI configuration:

   SpiHandle.Instance = SPI2;

   SpiHandle.Init.Mode = SPI_MODE_MASTER;

   SpiHandle.Init.Direction = SPI_DIRECTION_2LINES;

   SpiHandle.Init.NSS = SPI_NSS_SOFT;

   SpiHandle.Init.CLKPolarity = SPI_POLARITY_LOW;

   SpiHandle.Init.CLKPhase = SPI_PHASE_1EDGE;

   SpiHandle.Init.TIMode = SPI_TIMODE_DISABLE;

   SpiHandle.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;

   SpiHandle.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_64;

   SpiHandle.Init.DataSize = SPI_DATASIZE_8BIT;

   SpiHandle.Init.FirstBit = SPI_FIRSTBIT_MSB;

   SpiHandle.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

   SpiHandle.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;

   SpiHandle.Init.CRCPolynomial = 7;

   GPIO_InitStruct.Pin = GPIO_PIN_12;

   GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

   GPIO_InitStruct.Pull = GPIO_PULLUP;

   GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;

   GPIO_InitStruct.Alternate = GPIO_AF5_SPI;

   HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

   //MISO

   GPIO_InitStruct.Pin = GPIO_PIN_14;

   GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

   GPIO_InitStruct.Pull = GPIO_PULLUP;

   GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;

   GPIO_InitStruct.Alternate = GPIO_AF5_SPI;

   HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

   //MOSI

   GPIO_InitStruct.Pin = GPIO_PIN_15;

   GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

   GPIO_InitStruct.Pull = GPIO_PULLUP;

   GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;

   GPIO_InitStruct.Alternate = GPIO_AF5_SPI;

   HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

   hdma_rx.Instance                 = DMA1_Stream3;

   hdma_rx.Init.Channel             = DMA_CHANNEL_0;

   hdma_rx.Init.FIFOMode            = DMA_FIFOMODE_DISABLE;

   hdma_rx.Init.FIFOThreshold       = DMA_FIFO_THRESHOLD_FULL;

   hdma_rx.Init.MemBurst            = DMA_MBURST_SINGLE;

   hdma_rx.Init.PeriphBurst         = DMA_MBURST_SINGLE;

   hdma_rx.Init.Direction           = DMA_PERIPH_TO_MEMORY;

   hdma_rx.Init.PeriphInc           = DMA_PINC_DISABLE;

   hdma_rx.Init.MemInc              = DMA_MINC_ENABLE;

   hdma_rx.Init.Mode                = DMA_NORMAL;

   hdma_rx.Init.Priority            = DMA_PRIORITY_HIGH;

   if ( SpiHandle.Init.DataSize > SPI_DATASIZE_8BIT )

   {

      hdma_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;

      hdma_rx.Init.MemDataAlignment    = DMA_MDATAALIGN_HALFWORD;

   }else{

      hdma_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;

      hdma_rx.Init.MemDataAlignment    = DMA_MDATAALIGN_BYTE;

   }

   if ( HAL_OK != HAL_DMA_Init(hdma_rx) ) { return (-1); }

   __HAL_LINKDMA(SpiHandle, hdmarx, hdma_rx);

   hdma_tx.Instance                 = DMA1_Stream4;

   hdma_tx.Init.Channel             = DMA_CHANNEL_0;

   hdma_tx.Init.FIFOMode            = DMA_FIFOMODE_DISABLE;

   hdma_tx.Init.FIFOThreshold       = DMA_FIFO_THRESHOLD_FULL;

   hdma_tx.Init.MemBurst            = DMA_MBURST_SINGLE;

   hdma_tx.Init.PeriphBurst         = DMA_MBURST_SINGLE;

   hdma_tx.Init.Direction           = DMA_MEMORY_TO_PERIPH;

   hdma_tx.Init.PeriphInc           = DMA_PINC_DISABLE;

   hdma_tx.Init.MemInc              = DMA_MINC_ENABLE;

   hdma_tx.Init.Mode                = DMA_NORMAL;

   hdma_tx.Init.Priority            = DMA_PRIORITY_LOW;

   if ( pSpiHandler->pHalHandler->Init.DataSize > SPI_DATASIZE_8BIT )

   {

      hdma_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;

      hdma_tx.Init.MemDataAlignment    = DMA_MDATAALIGN_HALFWORD;

   }else{

      hdma_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;

      hdma_tx.Init.MemDataAlignment    = DMA_MDATAALIGN_BYTE;

   }

   if ( HAL_OK != HAL_DMA_Init(hdma_tx) ) { return (-1); }

   // Associate the initialized DMA handle to the the SPI handle

   __HAL_LINKDMA(SpiHandle, hdmatx, hdma_tx);

   // rx

   HAL_NVIC_SetPriority(DMA1_Stream3_IRQn, 1, 0);

   HAL_NVIC_ClearPendingIRQ(DMA1_Stream3_IRQno);

   HAL_NVIC_EnableIRQ(DMA1_Stream3_IRQn);

   // tx

   HAL_NVIC_SetPriority(DMA1_Stream4_IRQn, 1, 0);

   HAL_NVIC_ClearPendingIRQ(DMA1_Stream4_IRQn);

   HAL_NVIC_EnableIRQ(DMA1_Stream4_IRQn);

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.