2018-11-22 7:10 AM
Hi,
I'm really struggling with this, I cannot find any reason for the problem I'm seeing, I've looked at the example code in the firmware packages and I have identical code to the examples.
I'm using HAL to configure the project, the RTC is clocked from LSE which is up and running.
I call:
MX_RTC_Init();
And I can see that the registers change as expected.
I then call:
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0x5000, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
Which should result the RTC_WKUP_IRQHandler being called, but it never is.
If I look after 10 seconds at the RTC status registers I can see that WUTF is set.
I've tried adding:
__HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);
In various places as it seems that may be required after reading around, but it makes no difference, I cannot get the interrupt to fire, other interrupts from other peripherals are working fine.
My HAL_RTC_MspInit has the following code:
__HAL_RCC_RTC_ENABLE();
HAL_NVIC_SetPriority(RTC_WKUP_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(RTC_WKUP_IRQn);
Any suggestions?
2018-11-29 8:48 AM
Hello @adrian ,
There is a problem in the "stm32l4xx_hal_rtc_ex.c" file within the new version of STM32CubeL4 V1.13.0: The macro '__HAL_RTC_WAKEUPTIMER_EXTI_ENABLE_IT();' is missing in the HAL_RTCEx_SetWakeUpTimer_IT function (for other devices than STM32L412xx/STM32L422xx).
To fix this issue: the macro __HAL_RTC_WAKEUPTIMER_EXTI_ENABLE_IT()" in the HAL_RTCEx_SetWakeUpTimer_IT function should be added instead of "__HAL_RTC_WAKEUPTIMER_EXTI_ENABLE_EVENT" ( in line 912)
Hope this helps you.
Please keep us informed about your update.
Kind Regards,
Imen
2018-11-30 9:50 AM
This did indeed fix the issue, I now get the Wakeup interrupt!
Many thanks
2018-12-03 12:10 AM
We have already passed this issue along to our development team for fix in the coming release.
Kind Regards,
Imen
2018-12-03 4:48 AM
I asked above about exti, and adrian answered
> The EXTI is set correctly.
which I assume he said after reading out and checking the relevant EXTI registers bits.
Or not?
JW
2018-12-03 4:50 AM
Apparently it wasn't, I must have looked at the wrong register as it looked like it was set, but clearly wasn't.
The fix correctly fixes it, sounds like you correctly identified it but I just didn't see it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.