STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to connect NUCLEO-G071RB with STM32CubeMonitor-UCPD

I purchased a NUCLEO-G071RB and X-NUCLEO-USBPDM1 to development of my project.​Then I wrote a sample program according to application note AN5418, but it doesn't recognize it as a connectable port to the UCPD monitor.​Is it related to HWBoardVersionN...

Sodag.1 by Associate II
  • 2462 Views
  • 8 replies
  • 0 kudos

Location of MAC address storage in stm32h7 memory

When configuring a network interface, there is usually a hard coded MAC address somewhere in a config file, which is used to setup the interface.In production this address needs to be unique (purchased). For example in some stm32f4 mcus, there is a s...

emcewees by Associate
  • 3004 Views
  • 3 replies
  • 0 kudos

LwIP IPV6 DNS query failed

I have LwIP running on STM32+Cellular modem. The network is fine for IPV4. Now I am enabling IPV6.I can see my IPV6 address assigned with my IPV4.However, when I use lwip_getaddrinfo to have DNS query, but lwip_getaddrinfo return failed.Any hints are...

jiangpen by Associate II
  • 1152 Views
  • 0 replies
  • 0 kudos

Resolved! How to use CMSIS 5.8.0 in the cubeIDE

Hi,I use the stm32f446re with the cubeIDE and would like to use FFT's with 16 bit float (arm_rfft_fast_f16) like in the CMSIS DSP 5.8.0.The older CMSIS library works fine with the other data types but i cant get the new (DSP 1.9.0) to work. I tried d...

MH081 by Associate
  • 2419 Views
  • 2 replies
  • 0 kudos

HAL_I2C_mem_read_dma return error

I'm connecting to a nucleo144 through configured pins and i2c connection a melexis 90640 (thermal scanner) I initially tried through Hal functions to call the device on the default address I had from the datasheet (0x33) but did not find it so I solv...

Icont.1 by Associate II
  • 3584 Views
  • 8 replies
  • 0 kudos

Resolved! Jump issue with custom bootloader (STM32H7)

Hello,I've made several bootloader in the past without so much problem in the past with F2, F4, F7, but this time, I have some serious troubles with a STM32H743BI :)The bootloader (using the first sector, 128kb) reads a bin file from the SD card and ...

jean by Senior
  • 7089 Views
  • 7 replies
  • 1 kudos

I want to send AT+CWLAP commands and put only WiFi names (excluding commands and addresses) in the array to display five on the board. Please recommend me how to use it. Also, we analyzed the pattern. Please tell me how to parse.

// I use this code. And stm32h750 B/D w/ Esp8266.UART_HandleTypeDef UART2_WIFI;uint8_t RX_Data[128];uint8_t RXD;uint8_t data[11]="AT+CWLAP\r\n";if(IndexCount >= 200){ IndexCount = 0; if(StartFlag == 0) {  HAL_GPIO_WritePin(GPIOH,GPIO_PIN_10,GPIO_PIN_...

wwgww by Associate II
  • 786 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.