2019-05-29 2:15 AM
I have a question concerning the stm32f4xx_hal_i2c.c. In the function HAL_StatusTypeDef HAL_I2C_Master_Transmit(..) there is the following code sequence.
uint32_t tickstart = 0x00U;
/* Init tickstart for timeout management*/
tickstart = HAL_GetTick();
if(hi2c->State == HAL_I2C_STATE_READY)
{
/* Wait until BUSY flag is reset */
if(I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_BUSY, SET, I2C_TIMEOUT_BUSY_FLAG, tickstart) != HAL_OK)
{
return HAL_BUSY; -> return HAL_TIMEOUT
}
In my opinion instead of return HAL_BUSY it should return HAL_TIMEOUT because the function I2C_WaitOnFlagUntilTimeout checks for the timout to occur.
Can you please verify that and response to my question.
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.