2024-11-08 11:55 AM - last edited on 2024-11-08 12:06 PM by Tesla DeLorean
I had debugging problems with a H7 target, and by stepping thru the boot process I found the following line in SystemInit():
/*
* Disable the FMC bank1 (enabled after reset).
* This, prevents CPU speculation access on this bank which blocks the use of FMC during
* 24us. During this time the others FMC master (such as LTDC) cannot use it!
*/
FMC_Bank1_R->BTCR[0] = 0x000030D2;
At this stage of the boot process, the FMC power is not enabled, and thus reading or writing the register has no effect. Am I overseeing something or is this line for confusion?
Solved! Go to Solution.
2024-11-08 12:03 PM - edited 2024-11-08 12:18 PM
Hello @JojoS ,
@JojoS wrote:
At this stage of the boot process, the FMC power is not enabled,
You mean FMC clock not the power but your comment makes sense as the FMC clock is enabled in SystemInit_ExtMemCtl(), just after.
I will escalate this remark internally and get back to you as soon as I have an answer. Internal ticket number for follow up: 196021
2024-11-08 12:03 PM - edited 2024-11-08 12:18 PM
Hello @JojoS ,
@JojoS wrote:
At this stage of the boot process, the FMC power is not enabled,
You mean FMC clock not the power but your comment makes sense as the FMC clock is enabled in SystemInit_ExtMemCtl(), just after.
I will escalate this remark internally and get back to you as soon as I have an answer. Internal ticket number for follow up: 196021
2024-11-08 12:05 PM
>> Am I overseeing something or is this line for confusion?
Are you easily confused, is it a problem?
Probably there due to the generic way in which ST builds these thing, and perhaps salient to one particular case.
Perhaps so when built as a secondary application the loader has already started the clocks, external memories, etc prior to getting here.
Which file/project was this lifted from? An EVAL / DISCO board?
The SystemInit() in ARM's model would be used to bring up the whole board and memories so startup.s code can copy statics, etc.
2024-11-08 2:05 PM
Thanks, of corse it as a minor issue as it should have no affect. But it would be clearer if it is conditionally inserted.
2024-11-13 6:12 AM
FYI,
Issue confirmed and will be fixed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.