2020-06-19 10:48 AM
Hi
I am very new to write a code for USB communication. I am looking for helpful link or resource in setting up USB based camera communication over ethernet.
I have the following questions
There is a in build camera module on EVAL board but my project requirement is to use a see3_cam camera and transmit its video frames over ethernet.
Any help will be really appreciated.
Thanks
2020-06-19 11:33 AM
Perhaps there are some commercial USB stacks that have richer examples, and consultants with specific competencies?
If it is a USB Camera, and you're connecting it to the board, you'd need to be a USB HOST.
You'd need to understand the class and protocol it is using. Perhaps look at LINUX sources for supporting said camera, for expectations and initialization specifics.
I suspect you'll need to send USB request packets to the required endpoints on the camera/device.
2020-06-19 11:40 AM
Thanks @Community member for the helpful suggestion.
I will do the search for USB Host and library required for initialization of camera.
Thanks again
2020-06-20 1:05 AM
Besides USB this will probably also be useful:
2020-06-20 5:48 AM
Thankyou @Piranha for the reply.
I will keep those instructions in mind for LWIP ethernet.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.