STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using with LwIP stuck the task

Hello,​I download a file from server with netcomm_recv.​l write in FreeRTOS, with several tasks.For this discussion, l have two tasks.One is general task and the other​ is for downloading the file from server.From the first task, there is a condition...

Lmali.1 by Associate III
  • 1180 Views
  • 1 replies
  • 0 kudos

Resolved! USB PD library Can't source higher than 5V

Hello,We are using x-cube-usb-pd v3 library to implement source/sink application for our product. We've ported it to use on an STM32F030CC and using PTN5110 chip for TCPC controller. We are using configuration USBPD_TCPM_LIB_PD3_CONFIG_1.We have test...

Trying to flash a .dfu file containing micropython onto a nucleo-f767zi board, but have exhausted all options and I'm stuck.

I originally tried dfuse.exe, but it couldn't see the board when I plugged it in. The device shows up as a VCOM port under Ports in the windows 10 device manager list. Next I tried stm32 cube programmer, but in the instructions, it says to uninstal...

JBlac by Associate III
  • 7915 Views
  • 19 replies
  • 0 kudos

Resolved! STM32 USB Firmware update via High speed or Full speed?

Hello,Has anyone tried updating STM32 firmware over HS USB?I can't remember where I read it, but I remember the default STM32 DFU mode is only compatible with the FS USB.My device is a "USB Device" and it only needs HS USB to do the job, FS is not r...

BHan.1 by Associate II
  • 4158 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.