2025-07-11 7:45 AM
Hi Team,
I am working on SIL2/3 compliance project. For this I need to generate and work on LL based libraries instead of HAL libraries.
I am using STM32Cube v1.19.0. and working on STM32H753xx and STM32G4A1VET6 series MCU.
I am unable to generate LL libraries for FDCAN.
Need your help support for generating LL based FDCAN libraries.
Regards,
Abey
Solved! Go to Solution.
2025-07-11 5:55 PM
There is no LL FDCAN library on STM32H7. Only HAL.
2025-07-11 8:10 AM
Not sure what you mean by, "generate LL libraries" ?
The LL code is provided by ST in the firmware pack - you don't "generate" it.
2025-07-11 5:55 PM
There is no LL FDCAN library on STM32H7. Only HAL.
2025-07-14 12:21 AM
Thank you @TDK
For SIL2/3 compliance, "HAL" library-based coding Standard is acceptable?
If not, what are the other coding standard options for SIL2/3 compliance-based project?
Regards,
Abey
2025-07-14 6:22 AM
2025-07-14 10:44 AM
Yes,,our team connected with ST supplier for signing NDA to get the functional safety libraries. This process is in progress.
Meanwhile, we are working on the FDCAN config and communication establishment for STM32H7 and STM32G4 series.
But we need ST support team to confirm if, "HAL" library-based coding Standard is acceptable for SIL2/3 compliance or not?
If not, what are the other coding standard options for SIL2/3 compliance-based project?
This is important for us to align on coding standard.
2025-07-14 10:50 AM
Your original question is answered. Nothing about SIL in the OP.
If you have a new question, perhaps raise a new issue.
This is a community forum and isn't a direct line to ST support. If you want to submit a ticket, consider doing so here:
SIL compliance is more than just a check-the-box exercise based on which library you use.
2025-07-15 6:52 AM
Thanks @TDK
I will connect with ST team. Thanks for the link you shared.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.